bus object
    Defines the logical topology of a set of connected devices, including the buses that connect devices.
bus [busType] [name] { <property name> := <property value>; ... <device>.<port> ... }
| Property | Description | 
|---|---|
| busType (required) | Type of bus. | 
| name (required) | Name of the bus. The name is auto generated: <busType name> +<sequential number>  | 
| busSize | Configured size of the bus. This property defines how many child devices can be connected at once. The min and max bus size is defined in the busType. Validations are included to give warnings or errors when this value is out of range. | 
Provide Feedback