Smart Object properties
    These are the Smart Object properties. 
| Element  | Description  | 
| Desc  | Description. Information that describes the Smart Object. | 
| Version  | Version information for the Smart Object. Each revision number can be 0 to
                  999. If there is no period, the number is treated as a major revision only.  | 
For examples of Smart Objects, see Specify unique Smart Object instance values.
Provide Feedback