Device Definition - New Relay dialog box
Up to six relays can be added (slots 1-6). Empty slots between relays is not supported. Safety relays or devices could be added in relay or GuardLink via right-click menu of the relay tree. The new relay or device will be added with a minimum available slot or node number.
Provide Feedback