Sampler

Info - Sampling status

(class 0x312, instance 1, attribute 15)
Sampling progress
Sampling Status encoding
Value
Sampling Status
0
Waiting
1
Reference run
2
Dist. arm positioned
3
Purge process
4
Suction process
5
Medium detected
6
Dose process
7
sampling Ok
8
sampling nOk
9
Sampling delay
10
Sampling
11
Pre rinsing
12
Post rinsing
13
Launch bottle
14
Sample bottling
15
Emptying bottle
16
Rinsing bottle
17
Draining bottle

Info - Bottle configuration

(class 0x312, instance 1, attribute 9)
Bottle assignment
Bottle Configuration encoding
Value
Bottle Configuration
0
1x - PE Direct distribution
1
2x - PE Direct distribution
2
4x - PE/Glass-Schott Direct distribution
3
4x - Glass Direct distribution
4
12x - PE Direct distribution
5
12x - PE/Glass Plate distribution
6
24x - PE Direct distribution
7
24x - PE/Glass Plate distribution
8
6x+1x - PE/Glass Plate distribution
9
6x+2x - PE+PE Plate distribution
10
6x+2x - PE+Glass Plate distribution
11
12x+1x - PE/Glass Plate distribution
12
12x+2x - PE+PE Plate distribution
13
12x+2x - PE+Glass Plate distribution
14
12x+6x - PE Direct distribution
15
12x+6x - PE/Glass Plate distribution

Info - Bottle volume left

(class 0x312, instance 1, attribute 10)
Bottle volume
The value is transmitted in unit m3 (cubic meter) and displayed in unit mL (milliliter).

Info - Bottle volume right

(class 0x312, instance 1, attribute 11)
Bottle volume of the right bottle box
The value is transmitted in unit m3 (cubic meter) and displayed in unit mL (milliliter).

Info - Sampling technique

(class 0x312, instance 1, attribute 13)
Sampling mode
Sampling Mode encoding
Value
Sampling Mode
0
Peristaltic
1
Vacuum
2
Inline

Info - Dosing volume (vacuum/inline)

(class 0x312, instance 1, attribute 14)
Sampling volume
The value is transmitted in unit m3 (cubic meter) and displayed in unit mL (milliliter).

Manual Mode - Sample volume (peristaltic)

(class 0x312, instance 1, attribute 16)
The value is transmitted in unit m3 (cubic meter) and displayed in unit mL (milliliter).

Manual Mode - Sampling command

(class 0x312, instance 1, attribute 18)
Manual sampling command
Sampling Command encoding
Value
Sampling Command
0
---
1
Start
2
Stop

Manual Mode - Distributor position

(class 0x312, instance 1, attribute 17)
Distribution arm park position
Distributor Position encoding
Value
Distributor Position
0
Front
1
Bottle 1
2
Bottle 2
3
Bottle 3
4
Bottle 4
5
Bottle 5
6
Bottle 6
7
Bottle 7
8
Bottle 8
9
Bottle 9
10
Bottle 10
11
Bottle 11
12
Bottle 12
13
Bottle 13
14
Bottle 14
15
Bottle 15
16
Bottle 16
17
Bottle 17
18
Bottle 18
19
Bottle 19
20
Bottle 20
21
Bottle 21
22
Bottle 22
23
Bottle 23
24
Bottle 24
25
Back
26
Reference run

Manual Mode - Distributor parking

(class 0x312, instance 1, attribute 19)
Distributor Parking encoding
Value
Distributor Parking
0
---
1
Back

Program Mode - Program status

(class 0x312, instance 1, attribute 8)
Program state
Program Status encoding
Value
Program Status
0
Inactive
1
Active
2
Pause
3
Waiting for pause

Program Mode - Program name

(class 0x312, instance 1, attribute 7)
Name of current active program

Program Mode - Current program

(class 0x312, instance 1, attribute 1)
Program name

Program Mode - Current bottle

(class 0x312, instance 1, attribute 2)
Current bottle position

Program Mode - Bottle fill level

(class 0x312, instance 1, attribute 12)
Liquid level of selected bottle
The value is transmitted in unit m3 (cubic meter) and displayed in unit mL (milliliter).

Program Mode - Sampling mode

(class 0x312, instance 1, attribute 3)
Mode of sampling
Sampling Mode encoding
Value
Sampling Mode
0
Time paced CTCV
1
Flow paced VTCV
2
Time/flow paced CTVV
3
Single sample
4
Sampling table
5
External signal
6
Manual
7
EtherNet/IP

Program Mode - Next sample (Flow)

(class 0x312, instance 1, attribute 6)
The sampling is started when the parameterized volume is reached. This parameter displays the current value of the volume counter. The value is transmitted in m3 (cubic meter) and displayed in m3 and additionally in the unit gallon (U.S.). The translation faktor is: 1 m3 = 264.172052358 gallon (U.S.)

Program Mode - Next sample (Date)

(class 0x312, instance 1, attribute 4)
Date and time of next sampling

Program Mode - Next sample (Time)

(class 0x312, instance 1, attribute 5)
Date and time of next sampling
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal