Loading
Mutibelt | Transport | Kinetix | Studio 5000

Multibelt Transport System

Revision: A (05/04/2023) - Deploy Time: 30 Minutes | Learn how B5it works, how to apply and configure our specific libraries for multibelt systems
packaging line food and beverage industry
On This Page:
  • What is this for?
  • Installation guide
Innovation Center Home

What is this for?

The Multibelt system is a storage/transport system and consists of two or more independently driven belts. Each belt contains two or more trains (collators) that are built to carry a tray or built for a variable number of pockets. Trains vary in mechanical design. In the case of using a tray, the tray is placed inside the train in the loading position by any loading module. Products are fed from an infeed conveyor to the train at the filling position. If the feed train is full, it moves to the unloading position. If this is done, the train moves in positive rotation (recovery motion) behind the next train. This sequence guarantees a continuous flow of product in the filling area, while the other trains can be loaded with a tray and unloaded passing through the unloading position. The Multibelt equipment module can be configured with a large number of parameters, which are described in other chapters. A standardized interface for the load, supply and output module allows flexible adaptation. 

General Features

The  Multibelt System module concludes the following features:

• Multibelt storage sequence procedure for 2 axes (production mode)

• Automatic homing / reference move procedure

• Automatic synchronize move procedure

• Variable speed override adaption while production

• Jog function for each axis separately (service mode)

• Handling of multiple trains per belt

• Interface data handling to any other loading, infeed and outfeed module device

• Wide range of parameters to configure the module

Advantages:

The Mutibelt system has the advantage of being flexible and with the possibility of adaptation according to the application needs - number of collators (train).

From a software point of view, the system is relatively easy to implement using specific AddOn and Data DataTypes: Multibelt_AOI and Q_MAM_P (developed for this application, in order to reduce configuration, commissioning and startup time.

Limitations/Disadvantages

• Speed – Depends on the Drag Mechanism

• Number of mechanical elements - gears, belts

• Fixed space between cleats, if need change, mechanical change neededc

Is this useful for me?

In general, multibelt systems can be recommended to OEM manufacturers such as:

  • Conveyor belt manufacturers
  • Special machine manufacturers
  • Palletizers manufacturers
  • Packing machines manufacturers

Application areas:

Food, Manufacturing, Beverage

Benefits of applications with multibelt systems:

• Production gain and speed

• Increased dynamism in production

• 60% reduction in commissioning and startup time

• Easy of integration with devices: Robot, transfer devices

 

How can I make it work?

Requirements: Products, Tools, Previous Knowledge.

Hardware

  • Kinetix 5300, Kinetix 5500, Kinetix 5700 with CIP Motion and CIP Sync
  • PowerFlex 755 with Position control/ CIP Motion
  • CompactLogix L18ERM or high
  • Firmware revision 30 or high

Software

  • Logix Design Studio 5000
  • Program Multibelt_2Collators.ACD
  • AddOn instructions: Multibelt_AOI, Q_MAP_P

Knowledge

Intermediate knowledge of programming and configuration in Logix Design Studio 5000 software:

  • Ladder language (LD)
  • Motion configuration.

Downloads

Please note: You will need to agree to the Terms & Conditions for each download.

General_Files.zip ›
Legal Disclaimer Acceptance. ROCKWELL AUTOMATION WILL PROVIDE ACCESS TO ROCKWELL PRODUCTS (BEST PRACTICES, APPLICATIONS AND KNOWLEDGE) ON THE CONDITION THAT YOU ACCEPT AND COMPLY WITH THE FOLLOWING TERMS AND CONDITIONS. YOU ACCEPT AND AGREE TO BE BOUND BY THE TERMS OF THIS AGREEMENT BY DOWNLOADING, INSTALLING, COPYING, OR OTHERWISE USING PRODUCTS. IF YOU ARE ACCEPTING THESE TERMS ON BEHALF OF ANOTHER PERSON, COMPANY, OR OTHER LEGAL ENTITY, YOU REPRESENT AND WARRANT THAT YOU HAVE FULL AUTHORITY TO BIND THAT PERSON, COMPANY, OR LEGAL ENTITY TO THESE TERMS. IF YOU DO NOT AGREE TO THESE TERMS, DO NOT DOWNLOAD, INSTALL, COPY, ACCESS, OR USE THE PRODUCTS, SOFTWARE AND/OR CLOUD SERVICES. 1. Rockwell Automation retains full ownership and title to all Products and related documentation. No rights or licenses are granted other than those set forth in this Agreement. Company grants to Rockwell Automation a non-exclusive, worldwide, royalty-free, perpetual, non-revocable license to use any feedback Company provides regarding the Products, even if Company has designated the feedback as confidential. Rockwell Automation will be entitled to use the feedback without restriction or compensation to Company. 2. Company may not lease sub-lease, assign, license, sub-license or otherwise transfer any of the Products without the prior written consent of Rockwell Automation. Company may not assign or otherwise transfer access rights to the Products without the prior written consent of Rockwell Automation. Any reverse assembly, reverse engineering, decompilation, and creation of derivative works based on the Products by Company is prohibited. 3. Company acknowledges that Products provided under this Agreement are Rockwell Automation’s Confidential Information and are covered by effective or pending copyrights, patents, trademarks and/or trade secrets of Rockwell Automation, and Company agrees to maintain confidentiality by not disclosing Products or documentation to any third party without the prior written consent of Rockwell Automation and to protect the confidentiality of the Products as it would Company’s own confidential information. Company agrees that its obligation of confidentiality under this paragraph shall survive expiration or termination of this Agreement. 4. Company agrees that Products provided under this Agreement are prototypes and examples and its application and results may vary depending on each customer and project conditions. Rockwell Automation do not warranty the same results. This Agreement shall in no way be construed as a commitment by Rockwell Automation at any time to manufacture and/or offer Products for sale. There is no explicit or implicit service level agreement associated with using the Products. Rockwell Automation does not warrant that the functions contained in the Products will meet Company’s requirements. Company agrees to use all Products only in accordance with the instructions and only for the intended usages identified in the documentation. 5. EXCLUSION OF WARRANTIES AND LIMITATION OF LIABILITY. THE PRODUCTS ARE PROVIDED "AS IS". ROCKWELL AUTOMATION DISCLAIMS ANY AND ALL WARRANTIES, EXPRESS, IMPLIED OR STATUTORY, INCLUDING WITHOUT LIMITATION ANY WARRANTIES OF MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE. ROCKWELL AUTOMATION EXPLICITLY DISCLAIMS ALL WARRANTIES OF NON- INFRINGEMENT AND EXPRESSLY DOES NOT WARRANT THAT THE PRODUCTS, IN WHOLE OR IN PART, WILL BE ERROR FREE OR FREE FROM SECURITY VULNERABILITIES. IN NO EVENT SHALL ROCKWELL AUTOMATION BE LIABLE FOR (i) LOST PROFITS, LOST SAVINGS, DOWNTIME, SPECIAL, INDIRECT OR CONSEQUENTIAL DAMAGES OF ANY KIND, OR (ii) ANY PERSONAL INJURY, PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE ARISING OUT OF OR IN CONNECTION WITH THIS AGREEMENT, WHETHER IN AN ACTION IN CONTRACT, STRICT LIABILITY OR IN TORT INCLUDING NEGLIGENCE. 6. COMPANY AGREES TO INDEMNIFY AND HOLD ROCKWELL AUTOMATION HARMLESS FROM ALL COSTS, AWARDS, DAMAGES, EXPENSES AND FEES (INCLUDING ATTORNEYS FEES) RESULTING FROM OR RELATED TO ANY THIRD-PARTY CLAIMS (INCLUDING EMPLOYEES AND AGENTS OF COMPANY) AGAINST ROCKWELL AUTOMATION, ITS DISTRIBUTORS, AGENTS, OFFICERS, DIRECTORS OR EMPLOYEES FOR PERSONAL INJURY (INCLUDING DEATH), PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE RELATED TO OR RESULTING FROM THE USE OF THE PRODUCTS. 7. In the event a Product is exported, Company agrees to comply with all applicable United States Export Control Law and Regulations, and the applicable export control laws of other countries. This Agreement shall be governed by the laws of the state of Wisconsin. This Agreement is the complete and exclusive Agreement between Rockwell Automation and the Company, and supersedes all prior agreements, whether written or oral, relating to the Products.

Need Help?

If you need help with an application or have feedback from the Innovation Center, please contact us.

Installation Guide 

Additional information is in the "Multibelt.pdf" document in Downloads >> GeneralFiles.zip

Step 1:

Instructions:

  1. Open program Multibelt_2Collators.ACD – This file is located inside the Generalfiles.zip package in the Downloads section.
  2. Initially you can use this program with Virtual Axis for tests. After that you can couple the virtual axis with physical axis using Motion Axis Gear (MAG).
Step1.zip ›
Legal Disclaimer Acceptance. ROCKWELL AUTOMATION WILL PROVIDE ACCESS TO ROCKWELL PRODUCTS (BEST PRACTICES, APPLICATIONS AND KNOWLEDGE) ON THE CONDITION THAT YOU ACCEPT AND COMPLY WITH THE FOLLOWING TERMS AND CONDITIONS. YOU ACCEPT AND AGREE TO BE BOUND BY THE TERMS OF THIS AGREEMENT BY DOWNLOADING, INSTALLING, COPYING, OR OTHERWISE USING PRODUCTS. IF YOU ARE ACCEPTING THESE TERMS ON BEHALF OF ANOTHER PERSON, COMPANY, OR OTHER LEGAL ENTITY, YOU REPRESENT AND WARRANT THAT YOU HAVE FULL AUTHORITY TO BIND THAT PERSON, COMPANY, OR LEGAL ENTITY TO THESE TERMS. IF YOU DO NOT AGREE TO THESE TERMS, DO NOT DOWNLOAD, INSTALL, COPY, ACCESS, OR USE THE PRODUCTS, SOFTWARE AND/OR CLOUD SERVICES. 1. Rockwell Automation retains full ownership and title to all Products and related documentation. No rights or licenses are granted other than those set forth in this Agreement. Company grants to Rockwell Automation a non-exclusive, worldwide, royalty-free, perpetual, non-revocable license to use any feedback Company provides regarding the Products, even if Company has designated the feedback as confidential. Rockwell Automation will be entitled to use the feedback without restriction or compensation to Company. 2. Company may not lease sub-lease, assign, license, sub-license or otherwise transfer any of the Products without the prior written consent of Rockwell Automation. Company may not assign or otherwise transfer access rights to the Products without the prior written consent of Rockwell Automation. Any reverse assembly, reverse engineering, decompilation, and creation of derivative works based on the Products by Company is prohibited. 3. Company acknowledges that Products provided under this Agreement are Rockwell Automation’s Confidential Information and are covered by effective or pending copyrights, patents, trademarks and/or trade secrets of Rockwell Automation, and Company agrees to maintain confidentiality by not disclosing Products or documentation to any third party without the prior written consent of Rockwell Automation and to protect the confidentiality of the Products as it would Company’s own confidential information. Company agrees that its obligation of confidentiality under this paragraph shall survive expiration or termination of this Agreement. 4. Company agrees that Products provided under this Agreement are prototypes and examples and its application and results may vary depending on each customer and project conditions. Rockwell Automation do not warranty the same results. This Agreement shall in no way be construed as a commitment by Rockwell Automation at any time to manufacture and/or offer Products for sale. There is no explicit or implicit service level agreement associated with using the Products. Rockwell Automation does not warrant that the functions contained in the Products will meet Company’s requirements. Company agrees to use all Products only in accordance with the instructions and only for the intended usages identified in the documentation. 5. EXCLUSION OF WARRANTIES AND LIMITATION OF LIABILITY. THE PRODUCTS ARE PROVIDED "AS IS". ROCKWELL AUTOMATION DISCLAIMS ANY AND ALL WARRANTIES, EXPRESS, IMPLIED OR STATUTORY, INCLUDING WITHOUT LIMITATION ANY WARRANTIES OF MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE. ROCKWELL AUTOMATION EXPLICITLY DISCLAIMS ALL WARRANTIES OF NON- INFRINGEMENT AND EXPRESSLY DOES NOT WARRANT THAT THE PRODUCTS, IN WHOLE OR IN PART, WILL BE ERROR FREE OR FREE FROM SECURITY VULNERABILITIES. IN NO EVENT SHALL ROCKWELL AUTOMATION BE LIABLE FOR (i) LOST PROFITS, LOST SAVINGS, DOWNTIME, SPECIAL, INDIRECT OR CONSEQUENTIAL DAMAGES OF ANY KIND, OR (ii) ANY PERSONAL INJURY, PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE ARISING OUT OF OR IN CONNECTION WITH THIS AGREEMENT, WHETHER IN AN ACTION IN CONTRACT, STRICT LIABILITY OR IN TORT INCLUDING NEGLIGENCE. 6. COMPANY AGREES TO INDEMNIFY AND HOLD ROCKWELL AUTOMATION HARMLESS FROM ALL COSTS, AWARDS, DAMAGES, EXPENSES AND FEES (INCLUDING ATTORNEYS FEES) RESULTING FROM OR RELATED TO ANY THIRD-PARTY CLAIMS (INCLUDING EMPLOYEES AND AGENTS OF COMPANY) AGAINST ROCKWELL AUTOMATION, ITS DISTRIBUTORS, AGENTS, OFFICERS, DIRECTORS OR EMPLOYEES FOR PERSONAL INJURY (INCLUDING DEATH), PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE RELATED TO OR RESULTING FROM THE USE OF THE PRODUCTS. 7. In the event a Product is exported, Company agrees to comply with all applicable United States Export Control Law and Regulations, and the applicable export control laws of other countries. This Agreement shall be governed by the laws of the state of Wisconsin. This Agreement is the complete and exclusive Agreement between Rockwell Automation and the Company, and supersedes all prior agreements, whether written or oral, relating to the Products.
  • Step 1 - screenshot

    Step 1 - Image 1

  • Step 1 - screenshot

    Step 1 - Image 2

Screenshot of step 1, image 1
Screenshot of step 1, image 2

Step 2

Motion Configuration:

  1. Configure the Axes Parameters Virtual (Collator_X_AV) and Physical (Collator_X_AP) . For Physical: Model of operation: Position Loop.
  2. Configure the virtual axes.
  3. Couple virtual axis with real – This function is already in the program example (Multibelt_2Collators.ACD) .
  • Step 2 - screenshot

    Step 2 - Image 1

  • Step 2 - screenshot

    Step 2 - Image 2

  • Step 2 - screenshot

    Step 2 - Image 3

Step 2 - screenshot
Step 2 - screenshot
Step 2 - screenshot

Step 3:

Configure Add-ons Data parameters:

1. MainTask > MainProgram > _01_Multibelt, Configure Add-on MultiBelt_AOI.

  • Axis
  • Axis Preceding
  • Wagon Size
  • Number of Wagons
  • Loading Station Position
  • Waiting Station Position
  • Unloading Station Positions

2. MotionEventTask > Main_Motion_Rtn, configure Add-ON Q_MAM_P parameters (Setup and configure Train Data).

  • Axis
  • Axis Preceding
  • Command Position
  • Velocity
  • Acceleration
  • Deceleration 
  • Acceleration Jerk 
  • Decceleration Jerk
  • Step 3 - screenshot

    Step 3 - Image 1

  • Step 3 - screenshot

    Step 3 - Image 2

Step 3 - screenshot
Step 3 - screenshot

Step 4:

Download and commissioning

  1. You can use the Emulator (Factory Talk Logix Echo)
  2. For simulation, use MainTask > MainProgram > _02_Simulation program
  • Step 4 - screenshot

    Step 4 - Image 1

  • Step 4 - screenshot

    Step 4 - Image 2

Step 4 - screenshot
Step 4 - screenshot
Have a general inquiry?

Rockwell Automation and our partners offer exceptional industry knowledge to help design, implement, and support your automation investment.

Contact Rockwell Automation
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Sup...
  3. Chevron LeftChevron Left Pro...
  4. Chevron LeftChevron Left Downloads
  5. Chevron LeftChevron Left Innovation Center
  6. Chevron LeftChevron Left Multibelt Transport System