Downloads
What is it for?
The purpose of this solution is to support the development of Safe Zone Solutions using Laser Scanner and Safety Control Systems, enabling the compliance of various machines such as Robotic Cells, Conveyors, and mobile machines.
General Features
Sizing of Integrated Safety Solutions adopting current technologies and established concepts focused on applications in discrete manufacturing industries.
Advantages
- Compliance with the main current safety standards
- Use of certified safety solutions
- Solution enables greater production flexibility associated with safety
- Integrated Solution between Process and Safety
Limitations and Disadvantages
- Updated CCW software required
- Laser Scanner Programming Software must be up to date
- This is a standard sizing; installation definitions, input/output capacities, and safety classifications must be determined later
Need Help?
If you need help with an application or have feedback from the Innovation Center, please contact us.
Is this useful for me?
Sizing performed considering a Laser Scanner, Programmable Relay CR30, and direct start drives, which can also be done with Inverters or Servo Drives.
How can I make it work?
- Hardware: Standard computer or notebook and bill of materials.
- Software: CCW Connected Components Workbench and laser scanner programming software.
Installation guide
To implement, please follow the steps below.
Development of Safe Zone Applications using Laser Scanner
Version 1.0 - November 2025