View the Synchronization Log
On the Synchronization tab of the RMCT, you can view a log of synchronization events. If qualification of the redundant chassis pair fails, use the synchronization log to help identify and resolve the cause.
Synchronization Log

Parameter | Description |
|---|---|
Event No. | A unique, sequential number to identify the event. |
Time Stamp | The date and time that the event was logged. |
Basic Info | A basic description of the synchronization event. If qualification did not succeed or a fault is indicated, refer to the Extended Info columns to diagnose the cause. |
Extended Info 1 Extended Info 2 | Additional information that is related to the basic description of the event. Extended Info 2 information is not available for every event. |
Provide Feedback