Restrictions
IMPORTANT:
Motion is not supported in high availability systems. Delete motion groups, axes, and coordinate systems when redundancy is enabled.
The additional components are not supported in high availability systems:
- Event tasks
- Inhibited tasks
- License source control
- Consumed unicast connections. You can use produced unicast connections that remote consumers consume.
- Safety partner in a redundant chassis
- Produced safety tags
- Consumed safety tags
- OPC UA access
- Non-concurrent safety connections
- HMIBC and IOT instructions
- Match Project to Controller feature
- Bumpless output connections controlled by IOT instructions
- Listen Only connections forFLEX 5000®I/O
- Listen Only connections for highly integrated HART devicesThere is no ability for another controller to create Listen Only connections or dual-own these type of connections.
- Legacy communication networks that are connected to the redundant chassis pair:ControlNet®,DeviceNet®, RIO,DH+™.
For system component requirements and restrictions, such as communication modules and remote I/O modules, see System Components.
Provide Feedback