Configure Fiber Security

Fiber security enables secure communication between partner 1756-RM3 modules.
IMPORTANT:
Fiber security is enabled by default and can cause slower system performance, such as degraded scan time and qualification time. However, the switchover time is not affected.
To avoid impact to system performance, you can disable the feature.
Fiber security cannot be disabled or re-enabled if the redundancy system is in Protection Mode. To exit Protection Mode, disqualify the secondary chassis by using the Disqualify Secondary command on the Synchronization tab of the secondary redundancy module. For more information, see Protection Mode.
Whenever the fiber security configuration is changed, an event is logged in the event log.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal