Considerations for Communication Loss Diagnostics

The response time and diagnostic information for a loss of communication depends on the device and configuration settings.
Connection and Device Behavior
Type of Connection
Device Behavior
Direct connection to a controller
The device reports communication loss. The device communication loss can be replaced by the diagnostics of a communication adapter.
No connection to a controller
Communication adapters that do not have a connection to the controller do not report communication loss diagnostics. We recommend that you configure your communications adapters for a status connection to make sure that they report any communication loss diagnostic in a timely manner.
Data connection
The device reports communication loss. The device communication loss can be replaced by the diagnostics of a communication adapter.
Rack-optimized connection
The device does not report communication loss diagnostics. The communication adapter reports communication loss diagnostics. A device with a rack-optimized connection has a reduced set of diagnostics as compared to a direct connection.
When enabled, the Automatic Diagnostics feature enables the following:
  • Communication loss diagnostics for all devices in the controller I/O configuration.
  • Device-level automatic diagnostics evaluations for all uninhibited and enabled devices.
You can disable Automatic Diagnostics for a specific device in the device configuration. The communication loss diagnostic remains active even if the device disables Automatic Diagnostics. To disable communication loss diagnostic, inhibit the device or disable Automatic Diagnostics at the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal