Ladder Diagram Safety Instructions
Routines in the safety task can use the following types of ladder diagram safety instructions.
When instructions that result in values with decimal place are used with REAL or LREAL operands, Rockwell Automation has verified the precision to 6 decimal places.
Process
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
FGEN | Function Generator | Converts an input based on a piece-wise linear function. | Version 38 or later |
Advanced Math
Rockwell Automation has not done independent mathematical analysis of the numerical algorithms used in any of the following advanced math instructions. If you require a specific degree of accuracy, you must functionally test this instruction over your expected input domain.
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
EXPT | X to the Power of Y | Returns the value of X to the power of Y. | Version 36 or later |
XPY | X to the Power of Y | Returns the value of X to the power of Y. | Version 35 or earlier |
LN | Natural Log | Compute the natural log of a number. | Version 36 or later |
LOG | Log Base 10 | Compute the log base 10 of a number. | All versions |
Array (File)
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
AVE | File Average | Calculate the mean/average over a set of values. | All versions |
COP | Copy File | Copy binary data from one tag to another (no type conversion). When you use the COP instruction in a safety routine, you must verify that the length is a constant and that the source and destination length are the same. | All versions |
FAL | File Arithmetic and Logic | Perform copy, arithmetic, logic, and function operations on data that is stored in an array. | All versions |
FLL | File Fill | Fill the elements of an array with the source value, while leaving the source value unchanged. | All versions |
FSC | File Search and Compare | Compare the values in an array, element by element. | All versions |
SIZE | Size in Elements | Find the size of a dimension of an array. | All versions |
STD | File Standard Deviation | Calculate the standard deviation over a set of values. | All versions |
BSL | Bit Shift Left | Shifts the specified number of bits to the left. | All versions |
BSR | Bit Shift Right | Shifts the specified number of bits to the right. | All versions |
FFL | FIFO Load | Store a value into an array by using first-in/first-out semantics. | All versions |
FFU | FIFO Unload | Retrieve a value from an array by using last-in/first-out semantics. | All versions |
LFL | LIFO Load | Store a value into an array by using last-in/first-out semantics. | All versions |
LFU | LIFO Unload | Retrieve a value from an array by using last-in/first-out semantics. | All versions |
Bit
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
ONS | One Shot | Allows an event to occur one time. | All versions |
OSR | One Shot Falling | Sets an output bit for one scan on the true-to-false (falling) edge of rung state. | All versions |
OSF | One Shot Rising | Sets an output bit for one scan on the false-to-true (rising) edge of rung state. | All versions |
OTE | Output Energize | Controls a bit (it performs both Set and Clear operations based on rung state). | All versions |
OTL | Output Latch | Set a bit (retentive). | All versions |
OTU | Output Unlatch | Clear bit (retentive). | All versions |
XIC | Examine if Closed | Examines the data bit to set or clear the rung condition. | All versions |
XIO | Examine if Open | Examines the data bit to set or clear the rung condition. | All versions |
Time/Counter
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
CTD | Count Down | Count down. | All versions |
CTU | Count Up | Count up. | All versions |
RES | Reset | Reset a timer or counter. | All versions |
RTO | Retentive Timer On | Accumulate time. | All versions |
TOF | Off-delay Timer | Time how long a timer is disabled. | All versions |
TON | On-delay Timer | Time how long a timer is enabled. | All versions |
Compare
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
EQ | Equal To | Test whether two values are equal. | Version 36 or later |
EQU | Equal To | Test whether two values are equal. | Version 35 or earlier |
CMP | Compare | Perform a comparison on the arithmetic operations that you specify in the expression. | All versions |
GE | Greater Than Or Equal To | Test whether one value is greater than or equal to a second value. | Version 36 or later |
GEQ | Greater Than Or Equal To | Test whether one value is greater than or equal to a second value. | Version 35 or earlier |
GT | Greater Than | Test whether one value is greater than a second value. | Version 36 or later |
GRT | Greater Than | Test whether one value is greater than a second value. | Version 35 or earlier |
IsINF | Is Infinity | Check if floating point value is +/- infinity. | All versions |
IsNAN | Is Not a Number | Check if floating point value is Not-a-Number. | All versions |
LE | Less Than or Equal To | Test whether one value is less than or equal to a second value. | Version 36 or later |
LEQ | Less Than or Equal To | Test whether one value is less than or equal to a second value. | Version 35 or earlier |
LT | Less Than | Test whether one value is less than a second value. | Version 36 or later |
LES | Less Than | Test whether one value is less than a second value. | Version 35 or earlier |
LIMIT | Limit | Test whether a value falls within a specified range. | Version 36 or later |
LIM | Limit | Test whether a value falls within a specified range. | Version 35 or earlier |
MEQ | Mask Equal To | Pass source and compare values through a mask and test whether they are equal. | All versions |
NE | Not Equal | Test whether one value is not equal to a second value. | Version 36 or later |
NEQ | Not Equal | Test whether one value is not equal to a second value. | Version 35 or earlier |
Move/Logical
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
AND | Bitwise AND | Perform bitwise AND operation. | All versions |
CLR | Clear | Clear a value. | All versions |
MOVE | Move | Copy a value. | Version 36 or later |
MOV | Move | Copy a value. | Version 35 or earlier |
MVM | Masked Move | Copy a specific part of an integer. | All versions |
NOT | Bitwise Not | Perform bitwise NOT operation. | All versions |
OR | Bitwise Or | Perform bitwise OR operation. | All versions |
SWPB | Swap Byte | Rearrange the bytes of a value. | All versions |
XOR | Bitwise Exclusive Or | Perform bitwise exclusive OR operation. | All versions |
Program Control
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
AFI | Always False Instruction | Forces a rung to false (rung continues to execute). | All versions |
EVENT | Trigger Event Task | Triggers one execution of an event task. The event instruction triggers a scan of the standard task. | All versions |
JMP | Jump To Label | Scan of logic jumps to a labeled location within the same routine. | All versions |
JSR | Jump to Subroutine | Jump to a separate routine. | All versions |
LBL | Label | Identifies a target location for a JMP instruction. | All versions |
MCR | Master Control Reset | Forces every rung in a section of logic to execute in the False state. | All versions |
NOP | No Operation | Insert a placeholder in the logic. | All versions |
RET | Return | Return the results of a subroutine. | All versions |
SBR | Subroutine | Accept data that is passed to a subroutine by the JSR instruction. | All versions |
TND | Temporary End | Mark a temporary end that halts routine execution. | All versions |
Compute/Math
Rockwell Automation has done no independent mathematical analysis of the numerical algorithms used in the SQRT or SQR instructions. If you require a specific degree of accuracy, you must functionally test this instruction over your expected input domain.
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
ABS | Absolute Value | Take the absolute value of a value. | All versions |
ADD | Add | Add two values. | All versions |
CPT | Compute | Perform the arithmetic operation that is defined in the expression. | All versions |
DIV | Divide | Divide two values. | All versions |
MOD | Modulo | Determine the remainder after one value is divided by a second value. | All versions |
MUL | Multiply | Multiply two values. | All versions |
NEG | Negate | Take the opposite sign of a value. | All versions |
SQRT | Square Root | Calculate the square root of a value. | Version 36 or later |
SQR | Square Root | Calculate the square root of a value. | Version 35 or earlier |
SUB | Subtract | Subtract two values. | All versions |
Trigonometric
Rockwell Automation has not done independent mathematical analysis of the numerical algorithms in any of the following trigonometric instructions. If you require a specific degree of accuracy, you must functionally test this instruction over your expected input domain.
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
ACOS | Arc Cosine | Compute the arc-cosine of a number. | Version 36 or later |
ACS | Arc Cosine | Compute the arc-cosine of a number. | Version 35 or earlier |
ASIN | Arc Sine | Compute the arc-sine of a number. | Version 36 or later |
ASN | Arc Sine | Compute the arc-sine of a number. | Version 35 or earlier |
ATAN | Arc Tangent | Compute the arc tangent in radians of y/x based on the sign of a value to determine the correct quadrant. | Version 36 or later |
ATN | Arc Tangent | Compute the arc tangent in radians of y/x based on the sign of a value to determine the correct quadrant. | Version 35 or earlier |
ATAN2 | Arc Tangent 2 | Compute the arc tangent in radians of y/x based on the signs of both values to determine the correct quadrant. | All versions |
COS | Cosine | Compute the cosine of a number. | All versions |
SIN | Sine | Compute the sin of a number. | All versions |
TAN | Tangent | Compute the tangent of a number. | All versions |
I/O
For special considerations when using the GSV and SSV instructions, see the controller user manual.
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
GSV | Get System Value | Get controller status information. | All versions |
SSV | Set System Value | Set controller status information. | All versions |
Math Conversion
Mnemonic | Name | Description | Logix Designer Application |
|---|---|---|---|
DEG | Degrees | Convert radians into degrees. | All versions |
BCD_TO | Convert to Integer | Convert the BCD value to an integer value. | Version 36 or later |
FRD | Convert to Integer | Convert the BCD value to an integer value. | Version 35 or earlier |
RAD | Radian | Convert degrees into radians. | All versions |
TO_BCD | Convert to BCD | Convert the integer value to a BCD value. | Version 36 or later |
TOD | Convert to BCD | Convert the integer value to a BCD value. | Version 35 or earlier |
TRUNC | Truncate | Remove the fractional part of a value. | Version 36 or later |
TRN | Truncate | Remove the fractional part of a value. | Version 35 or earlier |
Provide Feedback