Configure the Safety Task Period and Watchdog

The safety task is a periodic timed task.
To configure the safety task period and watchdog, follow these steps.
  1. In the configuration tree, right-click the safety task.
  2. On the Task Properties dialog box, select the Configuration tab.
  3. Configure the parameters as described in Safety Task.
Safety Task Configuration
Safety Task Configuration
The priority of the safety task is not a safety concern, as the safety task watchdog monitors if a higher priority task interrupts the task. However, a higher priority safety task provides more consistent safety task performance. Safety Task priority = 1 is recommended.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal