Determine When I/O Data Is Updated
ControlLogix controllers update data asynchronously with the execution of logic.
Input Data Update Flowchart
Safety input tags (inputs, consumed, and mapped) are updated and frozen at the beginning of safety task execution.
Input Data Update
Output Data Update Flowchart
Output Data Update
Provide Feedback