Requirements for System Integrity
Security Component | Required to Meet IEC-62443-4-2 SL 1 | Details |
|---|---|---|
FactoryTalk® AssetCentre software | Yes | The FactoryTalk® AssetCentre server centrally tracks and manages configuration changes and restricts who can make changes based on FactoryTalk® Security settings. This server functionality assists with diagnostics and troubleshooting and reduces maintenance time for production assets.Configure the Device Monitor - Change Detect operation for the controller. For more information, see Configure System Security Features User Manual, SECURE-UM001 . |
FactoryTalk® Security software | ||
ControlFLASH Plus® software | Yes | Use ControlFLASH Plus® software to update controller firmware.Digitally signed firmware files have a .DMK (Device Management Kit) extension. ControlFLASH™ software authenticates the origin of a DMK file and validates the file before downloading in the device. |
Studio 5000 Logix Designer® application | Yes | You can generate a signature on an Add-On Instruction. This signature seals (encrypts) the Add-On Instruction to help prevent modification. |
Controller firmware update | Yes | To meet IEC-62443-4-2 SL 1 security requirements, you must use a certified version of the controller firmware. We recommend that you use the latest minor revision of your firmware. The controller is designed such that:
For more information, see Controller Firmware and Logix Designer Application Compatibility. |
CIP™ Bridging Control | May be required to maintain network segmentation. | CIP™ Bridging Control can be used to isolate secure and unsecure communication. For more information, see CIP Bridging Control. |
User-definable major controller faults | May be required based on system design, threat model, and risk assessment. | If your application requires a major fault in addition to those already monitored by the controller, define a predetermined state with a major fault so that outputs are off. For more information, see Configure User-definable Major Faults. |
(Safety-enabled controllers only). Safety signature | Yes for SIL 2 or SIL 3 configuration. | Safety-enabled controllers use a safety signature to verify the integrity of a safety application. The safety signature must be applied on a SIL 2/PLd or SIL 3/PLe safety-enabled controller to perform automated background integrity checks on the safety application. We recommend that you record and store the safety signature in a separate location to verify its integrity during audits or when tampering is suspected. |
Provide Feedback