Obtain Axis Information

You can obtain axis information by using these methods:
  • Double-click the axis (A) to open the Axis Properties dialog box.
  • Use a Get System Value (GSV) or Set System Value (SSV) instruction (B) to read or change the configuration at runtime.
  • View the QuickView pane (C) to see the state and faults of an axis.
  • Use an axis tag for status and faults (D).
Obtain Axis Information
An example of a project in Studio 5000 Logix Designer application showing the controller organizer, ladder logic, and QuickView pane.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal