Checklist to Develop a Safety Application Program
Use the following checklist to help maintain safety when you create or modify a safety application program.
✔ | System Requirements |
|---|---|
Does your controller support the version of the Studio 5000 Logix Designer® application used to create the safety application program? | |
Were the programming guidelines followed during the creation of the safety application program? | |
Does the safety application program contain only a ladder diagram? | |
Does the safety application program contain only safety instructions? | |
Does the safety application program clearly differentiate between safety and standard tags? | |
Are only safety tags used for safety routines? | |
Have you verified that safety routines do not attempt to read from or write to standard tags? | |
Have you verified that no safety tags are aliased to standard tags and vice versa? | |
Is each safety output tag correctly configured and connected to a physical output channel? | |
Have you verified that all mapped tags have been conditioned in safety application logic? | |
Have you defined the process parameters that the fault routines monitor? | |
Have you sealed any safety Add-On Instructions with an instruction signature and recorded the safety instruction signature? Optional for one time use Add-On Instructions. Required Add-On Instructions are reused on different applications. | |
Did you measure potential alarm bursts during system commissioning and change the project if measured scan times are not acceptable? | |
Has an independent safety reviewer reviewed the program, if necessary? | |
Has the review been documented and signed? |
Provide Feedback