Metal Form Instructions

AVC
Name
Description
AVC
Auxiliary Valve Control
Controls an auxiliary valve that is used with a main valve.
CBIM
Clutch Brake Inch Mode
Used for press applications where minor slide adjustments are required, such as press setup.
CBCM
Clutch Brake Continuous Mode
Used for press applications where continuous operation is desired.
CBSSM
Clutch Brake Single Stoke Mode
Used in single-cycle press applications.
CPM
Crankshaft Position Monitor
Used to determine the slide position of the press.
CSM
Camshaft Monitor
Monitors motion for the start, stop, and run operations of a camshaft.
EPMS
Eight-position Mode Selector
Monitors eight safety inputs to control one of the eight outputs that correspond to the active input.
MMVC
Maintenance Manual Valve Control
Used to drive a valve manually during maintenance operations.
MVC
Main Valve Control
Controls and monitors a main valve.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal