DIN Rail Mount the Supplemental Power Tap
- Pull each mounting clip away from the DIN rail as shown.IMPORTANT:Secure the DIN rail to a mounting surface approximately every 20 cm (7.87 in.) and use end-anchors appropriately.DIN Rail-mounted Supplemental Power Tap
- Place the power tap onto the DIN rail (TH35 per IEC 60715).
- Push each mounting clip toward the DIN rail.
- Use end anchors next to the left and right sides of the power tap to lock it into place on the DIN rail.
Provide Feedback