Connect the Supplemental Power Tap
- Insert the 1486-CON connector
with the attached 1486-CON flat cable media into the connection jack
on the power tap.
TIP:For a 1486-CON-P2L connector, make sure the etched arrow and cable are positioned left to right.For a 1486-CON-P2R connector, make sure the etched arrow and cable are positioned right to left.Connect the Supplemental Power Tap
Provide Feedback