Reseat the Communication Interface Module on a Push Button

  1. If the latch is not properly seated on the operator/panel, insert a small flathead screwdriver into the latch collar , then rotate the latch collar to the right .
    Applying pressure by hand is also an option to rotate the latch collar if a small flathead screwdriver is not available.
  2. To reseat the communication interface module, remove the latch with the module from the 800F operator.
  3. Insert a small flathead screwdriver into the lever on the bottom of the communication interface module.
  4. Gently pry the lever down until the communication interface module is released from the mounting latch of the 800F operator.
  5. Follow the steps in Connect an 800F Operator to the 800F Communication Interface Module to reinstall the module.
    Reseat Communication Module on Push Button
    Reseat Communication Module on Push Button
    Item
    Description
    Latch collar
    Rotate the latch collar
    Lever
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal