Set the IP Address for the Gateway

  1. Determine how you want to set the network IP address for the gateway: either rotary switches or a DHCP-supported method.
  2. Connect all supported devices to the gateway.
  3. Apply power to the gateway.
    When power is applied to the gateway:
    • A network IP address based on the rotary dials or via DHCP is assigned.
    • The gateway’s local
      EtherNet/IP
      In-cabinet system IP address of 192.168.1.1 is assigned.
    • Any user-defined devices on the local
      EtherNet/IP
      In-cabinet system are assigned IP addresses in ascending order (such as 192.168.1.2, 192.168.1.3, and 192.168.1.4).
    For an initial set-up of an
    EtherNet/IP
    In-cabinet system, the gateway automatically assigns IP addresses for supported devices on the local
    EtherNet/IP
    In-cabinet system.
    For a previously configured
    EtherNet/IP
    In-cabinet system, the gateway uses the user-defined reference topology.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal