Cabinet Mount the Gateway

  1. Place the gateway against the mounting surface.
  2. Check for level, then place a mark at each mounting hole location .
    Gateway Mount in Cabinet
    Gateway as mounted in a cabinet
  3. Drill holes at the marked locations.
  4. Align the gateway to the mounting holes, the secure them with two M4 or #8 screws and washers.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal