CIP Security
CIP Security™
is a standard, open-source communication mechanism that helps to provide a secure data transport across an EtherNet/IP™
network. CIP Security™
lets CIP™
-connected devices authenticate each other before transmitting and receiving data.CIP Security™
uses the following security properties to help devices protect themselves from malicious communication:- Device Identity and Authentication
- Data Integrity and Authentication
- Data Confidentiality
Rockwell Automation uses the following products to implement a
CIP Security™
solution:- FactoryTalk® Policy Managersoftware (includesFactoryTalk®System Services)
- FactoryTalk® Linxsoftware (lets workstation software communicate securely usingCIP Security™)
- Studio 5000 Logix Designer®application (This application required to interface withCIP Security™-enabled Logix controllers. The minimum application version varies by controller product family.)
For more information on
CIP Security™
, for example, a list of CIP Security™
-capable products and publications that describe how to use the products, including limitations and considerations, see the following:- Rockwell Automation Industrial Cybersecurity Solutions
- CIP Security with Rockwell Automation Products Application Technique, publication SECURE-AT001 (describes theCIP Security™-capable products, minimum software versions and product firmware revisions, and publications that describe how to use the products)
Provide Feedback