Starter Modes Depending on the Controlled-by Option
100-E and 104-E Starter Modes
The 100-E and 104-E starters operate as follows, depending on the ‘Controlled By’ option.
Controlled By | Peer Command | 100-E-INT-D | 104-E-INT-D | 100-E-INT-X | 104-E-INT-X |
|---|---|---|---|---|---|
Controller | None | ✔ | ✔ | ✔ | ✔ |
Controller/peer 2-wire | Run Forward | — | ✔ | — | ✔ |
Run Reverse | — | ✔ | — | ✔ | |
Stop | — | — | — | — | |
Hand | ✔ | ✔ | ✔ | ✔ | |
Off | ✔ | ✔ | ✔ | ✔ | |
Auto | ✔ | ✔ | ✔ | ✔ | |
Reset | — | — | ✔ | ✔ | |
Controller/peer 3-wire | Run Forward | ✔ | ✔ | ✔ | ✔ |
Run Reverse | — | ✔ | — | ✔ | |
Stop | ✔ | ✔ | ✔ | ✔ | |
Hand | ✔ | ✔ | ✔ | ✔ | |
Off | ✔ | ✔ | ✔ | ✔ | |
Auto | ✔ | ✔ | ✔ | ✔ | |
Reset | — | — | ✔ | ✔ | |
Peer 2-wire | Run Forward | ✔ | ✔ | ✔ | ✔ |
Run Reverse | — | ✔ | — | ✔ | |
Reset | — | — | ✔ | ✔ | |
Peer 3-wire | Run Forward | ✔ | ✔ | ✔ | ✔ |
Run Reverse | — | ✔ | — | ✔ | |
Stop | ✔ | ✔ | ✔ | ✔ | |
Reset | — | — | ✔ | ✔ |
Provide Feedback