Configure programs

Use the
Program Properties
Configuration
dialog box to assign routines and, under specific conditions, inhibit a program and synchronize redundancy data after execution.
To configure programs:
  1. From the
    Program properties
    dialog box, select the
    Configuration
    tab.
  2. Select the
    Main
    routine assigned to the program.
  3. Select the
    Fault
    routine assigned to the program.
  4. Select
    Inhibit Program
    to prevent the controller from executing this program. The option is cleared by default.
    This option is disabled if the
    Use as Folder
    check box is selected on the
    General
    tab.
  5. Select
    Synchronize Redundancy Data after Execution
    to synchronize data at the end of the program execution.
    This option is disabled when:
    • the
      Use as Folder
      check box is selected on the
      General
      tab
    • when Redundancy is not enabled
    This option does not appear for Safety controllers. The option is always enabled for controllers with Redundancy enabled as long as the controller is not in Hard Run mode.
  6. Select
    OK
    to save the program properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal