Show/Hide Sheet Boundaries command

Choose this command to display the sheet boundaries within a routine, based on sheet layout properties you have defined. You may display multiple sheets, with boundaries, within the sequential function chart routine window.
Using this command enables you to see where page breaks will be if and when you print our your routine(s), and to position language elements so that they are not split across multiple pages.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal