Initial Step command

Choose this command to designate this step as the first step at which the sequential function chart will begin executing after it has stopped and been restarted (e.g., as in a transition from Program mode to Run mode). This step is configured in the Restart Position setting on the SFC Execution tab of the Controller Properties dialog box.
TIP:
Only one initial step is allowed per sequential function chart routine. If you use this option to make a step the initial step, the
Logix Designer
application will automatically remove the initial step designation from any other step marked as the initial step.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal