Auto-Scroll command

Choose this command to enable the auto-scroll function during online monitoring. Enabling this command allows the sequential function chart routine to auto-scroll, so that the active step is always in view.
If there is more than one active step, the first active step is displayed at the top of the routine view, with as many of the others displayed in the view as the size of the window allows.
If there is no active step, choosing this command finds a step or a stop in the Reset state.
You can also use this command to find an active stop element.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal