Configure an MSG instruction tag

To configure an MSG instruction tag
:
  1. In
    Name
    , enter a name for the MSG instruction tag.
  2. In
    Description
    , enter a description for the MSG instruction tag (optional).
    The MSG instruction's tag Type, Data Type, and Scope display for your information.
  3. Select
    OK.
Access the Message Configuration dialog box, Tag tab
Select the
Tag Editor
to make it the active window, and then, select the to the right of the MESSAGE operand. From the
Message Configuration
dialog box, select the Tag tab. For more information, see Message Configuration Dialog Box - Tag Tab Overview
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal