Select Master Coordinated System Time

To select the master coordinated system time
  1. Right-click the
    Controller
    folder.
  2. Select
    Properties
    . The
    Controller Properties
    window appears.
  3. Select the
    Date/Time
    tab.
    If:
    And:
    Then:
    Your controller uses a motion axis
    No other controllers in your chassis are configured as the master controller
    • Select Make this controller the master
    • Select OK
    Your controller uses a motion axis
    Another controller in your chassis is configured as the master controller
    • Select OK
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal