Change Revision Dialog Box Overview

Use this dialog box to change the firmware revision for which the current project is configured.
Parameters
From
Lists the current major revision for which the project is configured.
To
Enter the number of the major firmware revision for which you want this project to be configured.
The list of available revisions includes all software major revisions that are installed, and that are greater than the current revision.
A backup of the project file is made with the old version in the name (for example, test_project.acd_v10).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal