Import Considerations when Replacing Components
When the name of a component being imported matches the name of an existing component of the same type and scope in the project, the components are said to collide and a connection is made. If there is no collision, the component is identified as needing to be created. If the component it connects to is incompatible (such as a tag of a different data type), then the connection is made, but a red flag indicates that there is a potential problem, and you must decide whether you wish to continue with the import or make additional configuration changes.
Generally, collisions can be managed by changing the Final Name or Operation setting for the content being imported.
Some of the collision decisions include:
Configuration | Description |
Import Name | The Import Name is read only and displays the name of the component as read from the import file. |
Operation |
|
Final Name | The Final Name determines the name of the component as it will appear in the project after the import (except in the case of deletes). Changing the Final Name changes the name in all places where this component is referenced in the import content. If you change the Final Name of the import content so that it newly collides with an existing component, all referenced components maintain any import configuration changes you might have already made. You can create or avoid collisions by changing the Final Name. If you change the final name to be different than the name in the import content, all logic references in the import content are updated to the new Final Name. In the Final Name and Alias For fields, some words auto-complete. These fields also distinguish between upper and lower case characters. |
Description |
|
Collision Handling
When there is a collision, the components colliding in the import file and in the project may be identically the same or they may be different. If they are the same, the Import Configuration dialog box defaults to Use Existing. If they are different, you must decide which definition you want to use. Icons on the Import Configuration dialog box show whether colliding components are identical or different. Reference component collisions default to Use Existing.
Situation | Icon |
The component only exist in the import file (creates). | The icon contains just the sheet of paper image. ![]() |
The component only exist in the project (deletes). | The icon contains just the cylinder image. ![]() |
The component collides with a different definition. | The icon contains both images with a collision symbol between the two images. ![]() |
The component collides with an identical definition. | The icon is blank (no difference). |
The component collides with an existing component and there are differences. | The icon contains both images, but no collision symbol. ![]() Note that this icon is always superseded by a red flag or red flag with a yellow triangle, if the attention flag applies to a particular item. |
This icon may appear in front of a folder in the Configuration Organizer tree if that folder contains a component where at least one of the following conditions exist:
| The icon contains both images, but no collision symbol, and displays to the left of the import component’s folder. ![]() Note that this icon is always superseded by a red flag or red flag with a yellow triangle, if the attention flag applies to a particular item. |
To see differences, press the Collision Details button on the imported component’s properties dialog box or the [...] button in the Collision Details column in the grid. Use this information on the differences to determine whether to overwrite or use the existing component.
For components that do not collide, press the Properties Details button for more information on the component.
Provide Feedback