View Safety Status and Signature
When there is a Safety controller, the controller safety status, safety lock state, and safety signature information can be viewed using the
Safety Status
button on the Online Bar and the Safety
tab on the Controller Properties
dialog. The Safety signature consists of an ID, Date, and Time. The date and time values correspond to when the signature was generated. The ID is a unique value calculated by the controller over the memory contents at the time the signature is generated.
TIP:
have a 32 byte ID. Only the first 4 bytes of the ID display
on the screen. Select
to view and copy the entire 32 byte ID.
Compact GuardLogix
5380 and GuardLogix
5580 controllers
to view and copy the entire 32 byte ID.To view safety status and signature information:
- TheSafety Statusbutton on the Online Bar shows the safety status states, whether the controller is safety-locked or -unlocked, or faulted.
- Select theSafety Statusbutton to view the Safety signature when a Safety signature exists.
- Select theController Propertiesicon and then select theSafetytab to view the safety status and signature information on theController Propertiesdialog.
Provide Feedback