Alarm conditions for PDOSE
Use the
Alarms
tab on the PDOSE Properties
dialog box to define alarm conditions for Process Dosing (PDOSE) instructions.To define alarm conditions for PDOSE instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- SelectAlarms.
- Configure these settings:
- Use Alarm. Select to use the alarm. Alarm conditions are not evaluated when an alarm is not in use.
- Alarm. Enter descriptive text that appears for the alarm.
- Limit. For flow rate alarms, enter the flow rate threshold for raising the corresponding alarm in engineering units.
- State. The state of the alarm. Hover over the state icon to see a tool tip that describes the alarm state or fault status.An alarm can be in more than one state at a time. For example, an alarm can be in alarm, unacknowledged and suppressed; or it can be normal, acknowledged and shelved.Alarm state icons include:
- Normal, acknowledged (no icon).
- Normal, unacknowledged -

- In alarm, acknowledged -

- In alarm, unacknowledged -

- Suppressed -

- Shelved -

- Disabled -

- Alarm fault -

- To open theAlarm Propertiesdialog box for an alarm, select theConfigurationicon
. - To configure settings for all pre-defined alarms for a PDOSE instruction, selectSettings for all alarms. When this box is checked, changes made to these settings are applied to all pre-defined alarms:
- Class. A group name for related alarms. The class does not limit the alarms that an Alarm Summary object subscribes to. UseClassto filter the alarms that are displayed to the operator.
- Alarm group. A group name to help classify and sort alarms.
- . AFactoryTalk ViewcommandFactoryTalk Viewcommand that can be run on the operator station when the alarm notification appears. Enter the exact syntax for theFactoryTalk Viewcommand.
- To allow an operator to shelve an alarm, selectAllow operator to shelve alarm.
- To allow maintenance technicians to disable an alarm, selectAllow maintenance to disable alarm.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. When theLogix Designerapplication is online with the controller, displays the current device state.
- Device issues. When theLogix Designerapplication is online with the controller, displays fault conditions.
- SelectApply.
Provide Feedback