PAI thresholds and deadbands for control conditions
Use the
Control limits
tab on the PAI Properties
dialog box to configure thresholds and deadbands for control limits for Process Analog Input (PAI) instructions. To configure thresholds and deadbands for control conditions for PAI instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select theAdvanced > Control conditionstab.
- Configure these settings:
- Condition: Threshold. For each condition, enter the threshold in engineering units. Set the threshold to the range of the signal connected to the input PV value in engineering units for the High-High, High, Low, and Low-Low range thresholds.Use thePV unitsbox on theHMItab to label the engineering units.
- Condition: Deadband. For each condition, enter the deadband around control High-High, High, Low, and Low-Low range limits. The deadband defines a range above or below the threshold to prevent unwanted rapid switching of the status.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state, such asPV goodorPV uncertain.
- Device issues. Displays fault conditions, such asPV badorConfiguration error.
- SelectApply.
Provide Feedback