Update module firmware

Perform firmware updates to ensure the modules have latest firmware version installed.
To update the module firmware:
  1. Select the modules that require a firmware update, or click
    Select All
    to select all modules in the list. Click
    Clear All
    if you want to deselect all modules.
    Modules that need firmware updates display as selected [ ] in this Grid view based on the following rules:
    • Controller - major revision of the firmware does not match
    • Motion Module - major revision of the firmware does not match Or - minor revision of the firmware does not match, and the module's Electronic Keying is set as Exact Match.
    • Sercos Drive - major revision of the firmware does not match Or - minor revision of the firmware does not match, and the module's Electronic Keying set as Exact Match.
    • CIP Motion Drives - major revision of firmware does not match Or - minor revision of the firmware does not match, and the module's Electronic Keying is set as Exact Match.
  2. For each selected module, from the
    Update To
    column, select a compatible revision from the list.
    Only the updates compatible with the version of software you are running appear in the table. The
    In Module
    column lists the current revision of firmware in the module.
    You can also click
    Browse
    to navigate to a specific directory.
  3. Click
    Update
    to start the flash upgrade. The firmware updates are completed in the order listed in the dialog box, beginning with the controller. Sercos Drives are listed under their parent 1756-Sercos Module, and are in alphabetical order sorted by the module name of the drive.
  4. To update Rockwell Automation Sercos Drives via ControlFLASH™, the 1756-Sercos module must be at least at Ring Phase=2, and Sercos ring connection must be maintained. The Sercos Drive LED will show Phase=5 during the Flash update period.
  5. Acknowledge the following warning dialog box.
    IMPORTANT: Do Not Remove Power While Updating Flash -- Motion On Any Axis on the Ring Will Be Stopped While Flashing for each and every Sercos Drive that is to be updated via this Update Module Firmware method.
    To make use of the Flash update of the Rockwell Automation Sercos Drives:
    • The Logix 1756-MxxSE module must have at minimum firmware revision 15.06, and
    • The Kinetix Sercos drives must have revision 1.85 or higher,
    • The 8720MC Sercos drives must have revision 3.85 or higher,
    • The Ultra Sercos drives must have revision 1.50 or higher.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal