Accept Instruction Modifications

Editing the instruction’s Mnemonic field changes the instruction type. When this change (Morphing) takes place, the operands remain in the same order (fore example, Operand 1 of original is Operand 1 of Morphed).
Examples (in ASCII):
Original Instruction
Morph To
New Instruction
TON Op1 Op2
XIC
XIC Op1
XIC Op1
TON
TON Op1 ?
TON ? OP2
XIC
XIC ?
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal