Change Cross Reference Report Preferences

To change cross reference report preferences:
  1. Select the
    Cross Reference
    category. Select or clear:
    These preferences apply to cross reference listings from the cross reference window.
    • Include tag cross reference
      - indicates that the tag cross reference table includes the cross reference for the tags.
    • Exact Match
      - select whether the cross reference is an exact match, which removes all alias tag information from the report.
  2. Select
    OK
    to accept the edits and close the
    Print Options
    dialog box.
Accessing the Print Options dialog box
To access the
Print Options
dialog box, from the
File
menu, choose
Print Options
. This dialog box is also accessible from the
Print
dialog box. Select
Print Options
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal