Select File Dialog Box
Use this dialog box to add project documentation translation to the project using a localization file.
Parameters
Parameter | Description |
|---|---|
Look in: | Select the directory where the localization file resides. |
Go to Last Folder Visited | Open the last visited folder. Enabled only if visited other folders and not at the default location for the dialog box. |
Up One Level | Move up one level in the directory tree. |
Create New Folder | Create a new folder in the current directory. |
View Menu | Select folder view (thumbnails, tiles, icons, lists, or details) |
File name: | Enter the name of the localization file to import. |
Files of type: | Choose the file type to import. Logix Designer Unicode Import/Export Files (*.TXT) is the only available choice. |
Import | Import the specified file. |
Cancel | Cancel the import and close the Select File dialog box. |
Help | View help about Select File dialog box. |
Provide Feedback