FactoryTalk® Twin Studio™ Release Notes
May 2024
FactoryTalk Twin Studio Release version 5.0.3 maintenance release.
ID Number | Title | Description |
---|---|---|
3378166 | When you start an Arena or Logix session in Twin Studio you may see an intermittent error message which states "The device is not ready." | This issue has been corrected. |
January 2024
FactoryTalk Twin Studio Release version 5.
Features and Enhancements
- Updated versions and packages for Emulate3D. Quick Access users can now use Emulate 3D v16.01.05 and associated packages.
- Updated Twin Studio quick access to use Logix designer v.36 in Logix Designer and Emulate3D applications.
- Windows patched images have been updated. All images are patched to the latest available patch Microsoft Windows Server 2019 Data center, version 10.0.17763 N/A build 17763
- Improved responsiveness.
- Visual improvements and icon redesign.
The following anomalies have been corrected in this release:
ID Number | Title | Description |
---|---|---|
3106587 | Layout issues when choosing a tier. | When choosing a tier text was moving off the page for smaller views. It now shifts left to remain visible. |
3114585 | Cross browser support in Mozilla Firefox. | The Twin Studio web page was not opening in the Mozilla Firefox browser. This has been corrected. |
2344705 | Navigation Issues when uploading project. | In some cases while attempting to upload a project and refreshing the page, a white screen that could not be interacted with would appear. This has been corrected. |
October 2023
First public release of FactoryTalk Twin Studio!
Features
FactoryTalk® Twin Studio™ is an end-to-end automation design solution where users can design, program, simulate, emulate and virtually commission in one cloud environment. This cloud-hosted ecosystem enables you to work within and move seamlessly between FactoryTalk Arena®, Studio 5000 Logix Designer®, FactoryTalk® Logix Echo, Emulate3D™ design solutions, and FactoryTalk View Machine Edition, all while collaborating with teammates in real time.
Provide Feedback