- Software components setup and installation
Ubuntu 22 keys reference table
During a connection to the Runtime of an Ubuntu 22 device through the
Remote desktop
, the input of some keys displays slightly inconsistently when using an English (United States) US keyboard. Use the following table for reference:Input | Display on the Ubuntu 22 device |
---|---|
`~ | ;: |
\| | `~ |
]} | =+ |
[{ | -_ |
;: | [{ |
/? | \| |
Provide Feedback