Best Practices

Best Practices

  • In the case of software installations on Windows devices, a firewall in the network (it is best if the firewall is a hardware firewall) should be configured so that all connections from the Internet to the device are blocked. Only one outgoing port should be used by
    FactoryTalk® Remote Access
    (TCP port 443, 80 or 5935) and kept open from the device to the Internet.
  • Windows devices should only run controlled and safe software.
  • The
    FactoryTalk® Remote Access
    software should be updated in case security improvements are released.
  • Given the suggestions made earlier, and given a proper, static and controlled industrial environment, an antivirus software can be avoided.
  • A strong administrator password change per IEC 62443-3-3 is enforced to register a Router to an organization. Keep the administrator password safe and do not share it with unauthorized personnel.
  • FactoryTalk® Remote Access
    routers can be connected to the Internet through its WAN port.
    FactoryTalk® Remote Access
    routers don’t enable any service through that port and will only need an outgoing connection through to the configured outgoing port (TCP port 443, 80 or 5935). They basically don’t expose any surface to known attacks from the outside. We periodically test the latest version of the firmware stack against new kinds of attacks. However, for the best security, an additional specialized firewall hardware would achieve the best protection from the outside.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal