- Software components setup and installation
Authorization
FactoryTalk®
Remote Access™
The customer’s
organization contains all the organization resources: users, groups and devices. The
organization administrator can design the organization and its rules to map any Rockwell
Automation 9 Security Architecture kind of organizational structure. Specifically, new users
and groups can be created to map the organization properly and make configuration easier and
more scalable.
FactoryTalk®
Remote Access™
Policies and permission rules can be applied to single resources or folders to apply them in a hierarchical way.
Finally, the Web API and the Access Server will enforce types of operations (such as remote desktop or file transfer) that will be allowed for a certain user of a certain resource (such as a remote device).
The online
help describes all the ways authorization rules can be configured.
FactoryTalk®
Remote Access™
Provide Feedback