- Software components setup and installation
Authentication
Use different types of authentication to help make sure that only authorized users have access to systems.
Authentication of Users to Servers
The users of
FactoryTalk®
Remote Access™
can sign in to the service by using their FactoryTalk®
Hub™
supported credentials.Authentication of Runtimes to Servers
When the Runtime
connects to the Access Server for the first time, it obtains a signed identity file that
contains the device UID in the domain.
The certificate is used for authenticating devices to the server and relies on the operating
system file system security. The certificate file is only accessible by elevated
processes.
FactoryTalk®
Remote Access™
FactoryTalk®
Remote Access™
FactoryTalk®
Remote Access™
FactoryTalk®
Remote Access™
FactoryTalk®
Remote Access™
Authentication of Access Servers to frontends and Runtime
As mentioned, clients use TLS 1.2 for connecting to Access Servers. Access Servers use an SSL server certificate signed by a well-known certificate authority. Clients can verify the signature against the certificate authority certificates installed in the system.
Provide Feedback