How to implement any network safety settings

How to implement any network safety settings

FactoryTalk® Remote Access
Manager
support firewall policies to help protect your network traffic. You can define or customize firewall rules or use any pre-set firewall policies including specific set of rules to allow for packets filtering.
  1. Access
    FactoryTalk® Remote Access
    Manager
    and the
    Domain view
    section.
  2. Click on the
    Add resource
    (
    circled plus
    icon) next to the folder or device for which you wish to activate a firewall.
  3. You can create or import firewall rules, depending on whether you wish to create a policy by customizing rules or use an existing set of rules.
    1. To import a firewall policy from the
      FactoryTalk® Remote Access
      Manager
      server, click on the circled plus icon next to a folder or a device and select
      Import firewall policy
      .
      1. Select the firewall policy that you wish to associate with your folder or device.
        NOTE: Children folders will inherit the firewall policy assigned to the related parent folder.
    2. To create a firewall policy, click on the circled plus icon next to a folder or a device and select
      Create firewall policy
      . Then, name the firewall policy and set firewall rules as needed.
NOTE: See Firewall settings for further information on this topic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal