Runtime launch

If you start your application as a service, Runtime launches automatically, without the need for a user to log in. In this case, you cannot use a Native Presentation Engine. The Runtime will work regardless of whether you have a user interface, for example, in the case of a gateway.
TIP: See
Configure a presentation engine
in the
FactoryTalk® Optix™
online Help.
If your application does not run as a service, you must login to allow Runtime to launch.
  1. Once you have installed the Runtime Tools, click
    Configure
    to launch them and select
    Run FactoryTalk Optix as a service
    .
  2. Deploy application to the target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal