Create a button that animates the image

Create a button that animates the image

  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Base controls
    Button
    .
  2. In
    Properties
    , in
    Text
    , enter
    Animate image
  3. In
    Events
    , next to
    MouseClick event
    , select
    Add
    and select
    UI
    MainWindow (type)
    rotateSVG
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal