Create a side menu

Create a side menu

  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Drawings
    Rectangle
    .
  2. (optional) Adjust the rectangle size as needed.
  3. (optional) Rename the shape accordingly.
  4. In
    Properties
    :
    1. Set a 
      Fill color
      .
    2. Set
      Left margin
      to
      -140
  5. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Base controls
    Button
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal