Create an event logger

Create an event logger

Create a logger that monitors the current temperature.
  1. In
    Project view
    , right-click
    Loggers
    and select
    New
    Event logger
    .
  2. Configure events:
    1. In
      Properties
      , next to
      Event configurations
      , select
      Add
      .
    2. Set
      Listen subtree
      to
      False
      .
    3. Set the
      Event type
      to
      AlarmConditionType
      .
    4. In
      Properties
      , double-click
      EventLogger1
    5. In the editor, select these variables:
      • BaseEventType
        Message
        .
      • BaseEventType
        Severity
        .
      • BaseEventType
        Time
        .
      • BaseEventType
        ConditionType
        AcknowledgeableConditionType
        AckedState
        Id
        .
      • BaseEventType
        ConditionType
        AcknowledgeableConditionType
        ConfirmedState
        Id
        .
      • BaseEventType
        ConditionType
        AcknowledgeableConditionType
        AlarmConditionType
        ActiveState
        Id
        .
    6. In the editor, select
      Apply
      .
  3. Create a dynamic link between
    Database
    and
    ProjectName
    DataStores
    EmbeddedDatabase1
    .
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal