Restore a project to a commit

Restore a project to a commit

Restore a previous version of a project.
TIP: When you restore a commit, the project in the local repository updates to include the contents of the selected commit. Restoring a commit permanently deletes any commits that occurred after the restored commit.
  1. From the toolbar, select
    View history
    .
  2. Select a commit to restore the project to.
  3. Select
    Restore
    .
Version history
closes and the open project includes the changes of the selected commit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal